PROFINET.ENISOWARNING
Description
This parameter allows warning 7012 (IRT configured without isochronous mode) to be disbaled. If for some reason the application does not require isochronous mode under conditions the drive would normally recommend it be enabled, this can be used to force the warning to become inactive.
Context
See warning W7012.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-03-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 0 or 1 |
Default Value | 1 |
Data Type | Integer |
Stored in Non-Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP
Fieldbus Information
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
PROFINET.ENISOWARNING |
3303 |
Unsigned8 |
Read/Write |
- |